Content originally posted in LPCWare by wwwenrico on Thu Apr 14 07:11:17 MST 2016
Hello,
I designed a board, based on the LPC2388, with an USB device interface.
The VBUS (pin P1.30) is used as an ADC and not as a VBUS detector.
QUESTION 1
Can I use a GPIO pin to detect the status of the VBUS?
QUESTION 2
Which software corrections I have to do to Keil HID demo program?
Thanks,
Enrico Migliore