Content originally posted in LPCWare by eeckenrode on Thu Feb 25 09:04:56 MST 2016
Hello,
We have a two board design where we connect a LAN8720A daughter board to a third party LPC2387 main board that we purchase. We have noticed some radiated emission issues to the point we cannot pass emission certifications for our product. The ENET_REF_CLK passes through a connect between the boards. This is the source of our emissions issue. We have been able to reduce emissions significantly by slowing the edges on the ENET_REF_CLK with a capacitor. We are looking for LPC2387 timing requirements for the MAC interface (in particular the ENET_REF_CLK) because we need to determine if we are violating any timing requirements. We are most curious if rounding the ENET_REF_CLK signal is a major concern?
-notes-
Placed a 47pF cap on ENET_REF_CLK. This essentially makes the clock signal mostly sinusoidal.
Trace lengths on Daughter Card - 0.25 inches (impedance matched)
Trace lengths on Main Board - 0.375 inches
Connector between boards
As tested with additional capacitor, signal integrity seems good and data transmission seems OK in the lab.
Thanks,
Eric