lpcware

LPC2362 Not entering ISP mode

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by jaisankar_av on Thu Jul 04 00:05:01 MST 2013

Hi,


I have a strange problem with my board LPC2362. The fresh controller is getting programmed for the very first time. And the second time onwards the controller is not entering into ISP mode.


I am using Flash magic for programming. RTS and CTS are included in the ISP connections and using via PC serial port.


I have probed the Reset pin and EINT(P2.10). Both are going LOW initially and then HIGH when trying to connect from flash magic, though not connecting on second attempt. The error I get is Failed to Autobaud.


First time after changing the controller, it works fine. So the ISP circuit is fine I guess.


Any valuable suggessions would be highly appriciated.


Thanks

Outcomes