Content originally posted in LPCWare by nerd herd on Wed Aug 27 09:52:54 MST 2014
Hello,
The main differences between the LPC11U68 and LPC11U67 is the flash memory, and the pin packages, but that should not affect the UART initialization process between the two. Have you made sure the pin you are probing is the pin you are initializing as UART1 TXD (PIO0_14)? Another thing to check is to try to initialize these pins as a GPIO and see if you can manually set and clear them to make sure the MCU can communicate with the pins. It wouldn't hurt to try initializing another UART on a different pair of pins as well. :)