Content originally posted in LPCWare by LyraElectronics on Wed Feb 04 09:46:56 MST 2015
I would like to programattically set the CAN module to be silent on the bus (no ACK, no transmit).
If I set the TEST bit in the CANCTRL register, and then set the SILENT bit in then CANTEST register, will the CAN module receive messages as normal thereafter?
If so, are there any disadvantages to leaving the TEST bit set during running?
Thanks,
Mike