I started with the blinky example and I want to programm it on a mbed lpc11u24 (using their online tool). I am messing with the board for a while without sucess. So my questions :
1- Is it possible load the code on an mbed devkit? 2- GPIOSetBitValue( 0, 7, 0 ); sets pin 7 low (and pin 7 is the one written 7 on my mbed board)?
The NXP bundle that you refer to uses the common libraries found in the common folder of the bundle. If you are going to use the online compiler you must add them to the project.