Yes, I was talking about s19 file, and was correctly generated, flash tool used the default output linker file in elf format, but i don't know if it's format is ok (it should be)
I tried with the S19 S-Record file, and I've got the same result :
Code:
========================================================================= Execute: Program=== Timestamp: Wed May 14 16:55:32 2008=== Flash Device: CFM_MCF52223=== Flash Organization: 8Kx32x1=== Flash Mem Start Addr: 0x00000000=== Flash Mem End Addr: 0x0003FFFF======================================================================Trying auto-detect...Auto-detection is successful. File is of type Motorola S-Record Format.Programming 0x00000418 bytes of Target Memory at 0x00000000Programming 0x00010000 bytes of Target Memory at 0x00004400Programming 0x00010000 bytes of Target Memory at 0x00014400Programming 0x00002618 bytes of Target Memory at 0x00024400Programming 0x00000036 bytes of Target Memory at 0x0003FFC0Flash Programmer: Flash driver reports the following error(s): Operation Unsupported Timed Out Verify failed Timestamp: Wed May 14 16:55:52 2008
It's not seems to be a file generation problem,.
Emmanuel