Content originally posted in LPCWare by rob.konieczny on Fri Apr 08 02:21:01 MST 2016
You're right. It works fine! Thank you for reply.
Solution was flashing LPC-Link2 probe with CMSIS-DAP firmware (latest LPC Scrypt used).
Before that, when I was trying to switch from SWD to JTAG I was getting error similar to that one (I can't remember exact).
Quote:
Use of JTAG with 'Keil ULINK-ME CMSIS-DAP' is not currently supported.
Reconfigure the Launch Configuration to use an SWD connection instead.
My understanding is that LPCXpresso IDE will soft-load CMSIS-DAP firmware. Flashing CMSIS-DAP firmware was even not advised in case probe is used only with LPCXpresso. Is there some difference between soft-loaded and flashed version of CMSIS-DAP?
I was using out-of-the-box LPCXpresso4337 and LPCXpresso 8.0.0 and 8.1.4.