Content originally posted in LPCWare by metraTec on Tue Feb 16 09:36:51 MST 2016
No, I'm not meaning that unit. I have seen the naming though.
I miss the SCB (known to me from LPC122x I worked with before) which I also found in the "core_cm0.h" and "core_cm4.h". Both entries differ a bit. I just copy the important things:
From "core_cm4.h":
/** \ingroup CMSIS_core_register
\defgroup CMSIS_SCB CMSIS SCB
Type definitions for the Cortex-M System Control Block Registers
@{
*/
/** \brief Structure type to access the System Control Block (SCB).
*/
typedef struct
{
__I uint32_t CPUID; /*!< Offset: 0x000 (R/ ) CPUID Base Register */
__IO uint32_t ICSR; /*!< Offset: 0x004 (R/W) Interrupt Control and State Register */
__IO uint32_t VTOR; /*!< Offset: 0x008 (R/W) Vector Table Offset Register */
__IO uint32_t AIRCR; /*!< Offset: 0x00C (R/W) Application Interrupt and Reset Control Register */
__IO uint32_t SCR; /*!< Offset: 0x010 (R/W) System Control Register */
__IO uint32_t CCR; /*!< Offset: 0x014 (R/W) Configuration Control Register */
__IO uint8_t SHP[12]; /*!< Offset: 0x018 (R/W) System Handlers Priority Registers (4-7, 8-11, 12-15) */
__IO uint32_t SHCSR; /*!< Offset: 0x024 (R/W) System Handler Control and State Register */
__IO uint32_t CFSR; /*!< Offset: 0x028 (R/W) Configurable Fault Status Register */
__IO uint32_t HFSR; /*!< Offset: 0x02C (R/W) HardFault Status Register */
__IO uint32_t DFSR; /*!< Offset: 0x030 (R/W) Debug Fault Status Register */
__IO uint32_t MMFAR; /*!< Offset: 0x034 (R/W) MemManage Fault Address Register */
__IO uint32_t BFAR; /*!< Offset: 0x038 (R/W) BusFault Address Register */
__IO uint32_t AFSR; /*!< Offset: 0x03C (R/W) Auxiliary Fault Status Register */
__I uint32_t PFR[2]; /*!< Offset: 0x040 (R/ ) Processor Feature Register */
__I uint32_t DFR; /*!< Offset: 0x048 (R/ ) Debug Feature Register */
__I uint32_t ADR; /*!< Offset: 0x04C (R/ ) Auxiliary Feature Register */
__I uint32_t MMFR[4]; /*!< Offset: 0x050 (R/ ) Memory Model Feature Register */
__I uint32_t ISAR[5]; /*!< Offset: 0x060 (R/ ) Instruction Set Attributes Register */
uint32_t RESERVED0[5];
__IO uint32_t CPACR; /*!< Offset: 0x088 (R/W) Coprocessor Access Control Register */
} SCB_Type;
/***********END******************/
From "core_cm0.h":
/** \ingroup CMSIS_core_register
\defgroup CMSIS_SCB CMSIS SCB
Type definitions for the Cortex-M System Control Block Registers
@{
*/
/** \brief Structure type to access the System Control Block (SCB).
*/
typedef struct
{
__I uint32_t CPUID; /*!< Offset: 0x000 (R/ ) CPUID Base Register */
__IO uint32_t ICSR; /*!< Offset: 0x004 (R/W) Interrupt Control and State Register */
uint32_t RESERVED0;
__IO uint32_t AIRCR; /*!< Offset: 0x00C (R/W) Application Interrupt and Reset Control Register */
__IO uint32_t SCR; /*!< Offset: 0x010 (R/W) System Control Register */
__IO uint32_t CCR; /*!< Offset: 0x014 (R/W) Configuration Control Register */
uint32_t RESERVED1;
__IO uint32_t SHP[2]; /*!< Offset: 0x01C (R/W) System Handlers Priority Registers. [0] is RESERVED */
__IO uint32_t SHCSR; /*!< Offset: 0x024 (R/W) System Handler Control and State Register */
} SCB_Type;
/***********END******************/
Also: in both:
#define SCS_BASE (0xE000E000UL) /*!< System Control Space Base Address */
#define SCB_BASE (SCS_BASE + 0x0D00UL) /*!< System Control Block Base Address */
Important things I miss:
CPUID, SLEEPDEEP bit (in SCR), AIRCR (for resetting)