LPC 4357

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 4357

256 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by imroun1992 on Wed Sep 18 14:31:58 MST 2013
Hello,

I put the datasheet now, can you help how to establish the I2C Communication between KEIL MCB 4357 and MPU 6050 accelerometer. I wan if it's possible a source code to initializing I2C Communication between these component and a code for initializing all axis of accelerometer.

http://dlnmh9ip6v2uc.cloudfront.net/datasheets/Components/General%20IC/PS-MPU-6000A.pdf

Thanks You

Average:
Labels (1)
0 Kudos
1 Reply

238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Sep 24 04:49:55 MST 2013
The documentation of the sensor is not very complex, there is a separate document describing the registers which you can read/write via I2C.
Invensense has an evaluation board in combination with an MCU from ATMEL. So you find a lot of websites dealing with it.
Simply Google for "ATMEL MPU6050" and you find them.
e.g. http://davidegironi.blogspot.com/2013/02/avr-atmega-mpu6050-gyroscope-and.html#.UkF6_z9xVv4

Regards,
NXP Support
0 Kudos