Content originally posted in LPCWare by mc1992 on Sat Nov 28 16:37:03 MST 2015 Hello, I am searching a library to use a lcd 16x2 with lpc4337. I appreciate your help. Bye :D!
Content originally posted in LPCWare by rocketdawg on Tue Dec 01 08:26:52 MST 2015 This display uses the ST7066 Controller which is very similar to the very common HD44780 controller. first google hit on the data sheet https://www.sparkfun.com/datasheets/LCD/st7066.pdf I found several github references with code samples and even sparkfun has sample code https://www.sparkfun.com/products/9053
the ST7066 ships in either a 5 V or a 3.3 V chipset. the only thing to be concerned with is whether the LCD is actually a 3.3 V device. If it is a 5 V device, it may or may not work at all.
Content originally posted in LPCWare by mc1992 on Mon Nov 30 19:41:11 MST 2015 I am using the 16x2 WH1602A display. For the communication I use the GPIO ports with the functions of "gpio_18xx_43xx.h" library to send bits to the LCD . Thanks! :bigsmile:
Content originally posted in LPCWare by mc on Mon Nov 30 18:39:11 MST 2015 Hi MC1992, Could you please let us know the details of LCD? What interface is used to communicate with LCD? SPI ?