Content originally posted in LPCWare by GTA on Tue Apr 15 03:20:40 MST 2014
Hello,
My company is working on a new design for high performance motor control. We would prefer to use an NXP MCU, equipped with a Cortex-M4F and fast, (at least) 12 bit ADCs. Additional cores are optional, but potentially useful for us. The LPC4370 is not a first-hand option due to only coming in BGA packages. An LPC1500 MCU, but equipped with a Cortex-M4F core would be very good.
Does NXP plan to release such an MCU in the foreseeable future?
We know there is the LPC4000 series, but we would like to have a higher ADC conversion rate than 400 kHz.
BR,