Hello, I am a total newbie when it comes to CodeWarrior. I have run across a problem in one of our very old projects. The project compiles fine with CodeWarrior 6.4. However, when I try and delete a file from the project screen, and then add it back, it claims it cannot find stdlib.h. I find this odd cause it can find stdio.h, which is located in the same folder.
Can anyone help?
Thanks for your help...
Yes-I am using CodeWarrior for ColdFire 6.4. I have no idea what version of CodeWarrior made the original project, as the code I am working with is many years old. I just recently tried porting the code to 7.0 (later had to settle with 6.4).
The source file with the problem simply uses:
#include <stdlib.h>
I tried removing the object code, resetting the entry paths, and re-searching for files (in that order). I still get the same error. I tried adding the compiler directory (MSL folder) to the project paths, and it still can’t find the file.