Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 20 15:12:37 MST 2013 I presume that you are asking if LPCXpresso 6 supports the use of LPC-Link2 to connect LPC18/43 targets - the answer to this is yes.
Content originally posted in LPCWare by whitecoe on Sun Sep 15 06:42:32 MST 2013 It is supported. I am happily using an LPC-Link2 with LPCXpresso IDE here. But the LPC-Link2 functionality in LPCXpresso just doesn't support LPC18/43 as a target MCU yet. - as stated in the FAQ that LPCXpresso Support pointed you at.
Content originally posted in LPCWare by mhelin on Sat Sep 14 13:09:44 MST 2013 Quote: lpcxpresso-support Not in the current LPCXpresso 5 release no. As per the other threads previously referenced and the below FAQ, LPC43 will be supported via LPC-Link2 in a forthcoming release.
Content originally posted in LPCWare by lpcxpresso-support on Sat Sep 14 06:18:59 MST 2013 Not in the current LPCXpresso 5 release no. As per the other threads previously referenced and the below FAQ, LPC43 will be supported via LPC-Link2 in a forthcoming release.
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 06 00:58:09 MST 2013 Just to expand on this response, the LPC4357 is already fully supported in the current LPCXpresso 5.2.6, but only using the original LPC-Link (or Red Probe+), not via LPC-Link2. There have been a number of threads about this recently ,if you browse or search the forum.
More generally information on LPC43 support can also be found at:
Content originally posted in LPCWare by lpcxpresso-support on Thu Sep 05 21:06:00 MST 2013 A new version of the LPCXpresso IDE, to be released very very soon, fully supports LPC4357.