Content originally posted in LPCWare by MikeSimmonds on Thu Sep 18 15:43:19 MST 2014
I am interrested in the LPC-Link2 board (4370)
If I enter ISP mode (with a low on the appropriate pin at reset) and write a program image
to sram at 10000000, and then 'Go'
What is to state of (a) the M4MEMMAP register and
(b) clock speed, clock source, PLL1 settings etc.
Do I have to transfer to an actual code address and setup my own SP,
or would a transfer to 1000000 take this as the vector table and set the
stack and initial PC from the first two entries?
Regards, MIke