lpcware

LPC4078 LQFP100: SPIFI + SD card at the same time?

Discussion created by lpcware Employee on Jun 15, 2016
Content originally posted in LPCWare by gjwep on Wed Apr 01 14:24:23 MST 2015
Hello,

I am using LPC4078 LQFP100 and I'd like to use SPIFI and the SD card interface. 

Per datasheet, the only pin that has SPIFI_CLK (P0.22) is also the only pin which has SD_DAT[0]. Is there a smart workaround to still be able to use both peripherals at the same time?

Any hints much welcome.

Thanks in advance,
gj

Outcomes