Content originally posted in LPCWare by rcsison on Mon Mar 26 12:19:04 MST 2012
With our phyCORE-LPC3250 Rapid Development Kit, our display works for 24bpp when specifying the screen at 160x160 (as an experiment). When doing this a 160x160-pixel Windows desktop comes out fine and functions correctly, in the upper-left-hand corner of the 800x600 screen (the only area painted).
When I go for higher dimensions (namely, widths approaching 800 pixels), a few lines are painted, but then the system hangs up (like it crashed).
Has anyone out there been able to run an 800x600 LCD at 24bpp with an LPC3250 or other type of unit?
Thanks for your help!