Content originally posted in LPCWare by dsidlauskas on Sat Jan 25 16:44:26 MST 2014
I have a new out of the box NGX LPC1857 board. I am using it with LPCXpresso and LPC-Link JTAG board.
I have built the NGX supplied projects, but when I go to flash them I get and error
Failed on connect: Ep(01). Target marked as not debuggable.
Connected. Was: None. DpID: EDB6. Info: HID64HS12[/color]
The detailed error message is:
crt_emu_lpc18_43_nxp -flash-load-exec "C:\Temp\workspace18\periph_atimer\Debug\periph_atimer.axf" -g -2 -vendor=NXP -
pLPC1830 -wire=hid -s250 -flash-driver=LPC18_43_SPIFI_4MB_64KB.cfx -x C:/Temp/workspace18/periph_atimer/Debug
Ni: LPCXpresso Debug Driver v6.0 (Dec 30 2013 11:03:08 - crt_emu_lpc18_43_nxp.exe build 1222)
Pc: ( 0) Reading remote configuration
Nc: Found chip XML file in C:/Temp/workspace18/periph_atimer/Debug/LPC1830.xml
Pc: ( 5) Remote configuration complete
Pc: ( 15) nSRST assert (if available)
Ed:02: Failed on connect: Ep(01). Target marked as not debuggable.
Et: Emu(0): Connected. Was: None. DpID: EDB6. Info: HID64HS12
Error 0: (null)
Last sticky: 0. AIndex: 0
No MemAp selected
I have no problem in using the LPC-Link on a LPC1769.
No Speed test
SWD Frequency: 50 KHz. RTCK: False. Vector catch: False.
Packet delay: 0 Poll delay: 0.
Pc: (100) Target Connection Failed
The NGX projects for the 1857 come with the MCU set for 18230. I have tried changing the MCU settings to 1857 but get the same result.
I would appreciate any suggestions or help.
Thanks.
Dave Sidlauskas