Hello LPC WARE
I have the same problem. I use the lpc4337. I want to use ADC0_0 (P4_3)and ADC1_0(PIN 6) at the same time .The two pins have been connectted to diffirent signals.But when I tested,I found that the two signals had been connectted together. I just want to know if the two pins can be used at the same time.If they can be used together,giving me some examples is better.
Regards,
Huixin Yang
With comment of Marion, I guess you can not use ADC0_0 and ADC1_0 in same time. It is connected physically inside chip and there is no way to use it independently. I also checked in my hardware during use ADC0_1 and ADC1_1 same time.
Jongkook