LCD Driver PCF8576D Sample Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD Driver PCF8576D Sample Code

658 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alan_nn on Tue Apr 01 04:34:59 CDT 2014
The PCF8576D is a Universal LCD driver for low multiplex rates, which could generates the drive signals for any static or multiplexed LCD containing up to four backplanes and up to 40 segments .This sample code demonstrate how to configure the display and operating mode of PCF8576D, also how to light on the relative segments to show “2014” on NXP OM6290 demo board.
Labels (1)
0 Kudos
1 Reply

509 Views
zafarobad
Contributor I

I can't find the sample code here ?

0 Kudos