Hello,
I'm trying to get the emWin BSP 5.20 for the EA 1788 Dev-Kit running on my Hitex LPC1850 EVA-Board. Both Boards uses the same Display: EA 7" LCD-Board. Now I have made the modifications in the BSP. The problem is that I can't download the project in the external flash (SST39VF3201).
My IDE is Code Red RedSuite 5.
I get the following error messages:
-> Flash Driver "Init" return error code 0x1 ;
-> Target reported errors, reason:15: Target error from commit flash write ;
-> Error in final launch sequence Failed to execute MI command: -break-insert -t main
Error Message from debugger back-end: cannot access memory at address 0x1c001f78
The parallel flash ram uses the same lines as the sdram. Could it be, that I have to switch between the memories? Did anybody have experiences with the Hitex EVAL Board and the usage of both memories? After building the Project I get an error: "make:***[NXP_Hitex1850_BSP_LPCXpresso510.axf] Error 1".
Please, can somebody help me with this problem?
Thanks.
Martin
Have you looked in the QuickStart guide for this board? It mentions in there how to set up programming external flash...
I tried to program a simple Code on the external flash to check if everything is still working and I got the same error... < Flash Driver "Init" return error code 0x1 > Could it be that I damaged the external flash?