/****************************************************************************
* $Id:: adc.c 6089 2011-01-06 04:38:09Z nxp12832 $
* Project: NXP LPC17xx ADC example
*
* Description:
* This file contains ADC code example which include ADC
* initialization, ADC interrupt handler, and APIs for ADC
* reading.
*
****************************************************************************
* Software that is described herein is for illustrative purposes only
* which provides customers with programming information regarding the
* products. This software is supplied "AS IS" without any warranties.
* NXP Semiconductors assumes no responsibility or liability for the
* use of the software, conveys no license or title under any patent,
* copyright, or mask work right to the product. NXP Semiconductors
* reserves the right to make changes in the software without
* notification. NXP Semiconductors also make no representation or
* warranty that such application will be suitable for the specified
* use without further testing or modification.
****************************************************************************/
#include "lpc17xx.h"
#include "type.h"
#include "adc.h"
#include "Variables.h"
#ifndef _BV
#define _BV(_x_) (1UL << (_x_))
#endif
//volatile uint32_t ADCValue[ADC_NUM];
//volatile uint32_t ADCIntDone = 0;
volatile uint32_t BurstCounter = 0;
volatile uint32_t OverRunCounter = 0;
#if BURST_MODE
volatile uint32_t channel_flag = 0;
#endif
#if ADC_INTERRUPT_FLAG
/******************************************************************************
** Function name:ADC_IRQHandler
**
** Descriptions:ADC interrupt handler
**
** parameters:None
** Returned value:None
**
******************************************************************************/
void ADC_IRQHandler (void)
{
uint32_t regVal;
volatile uint32_t dummy;
int i;
regVal = LPC_ADC->STAT;/* Read ADC will clear the interrupt */
if ( regVal & 0x0000FF00 )/* check OVERRUN error first */
{
OverRunCounter++;
for ( i = 0; i < ADC_NUM; i++ )
{
regVal = (regVal & 0x0000FF00) >> 0x08;
/* if overrun, just read ADDR to clear */
/* regVal variable has been reused. */
if ( regVal & _BV(i) )
{
dummy = LPC_ADC->DR;
}
}
LPC_ADC->CR &= ~((0x7<<24)|(0x1<<16));/* stop ADC now, turn off BURST bit. */
// ADCIntDone = 1;
return;
}
for ( i = 0; i < ADC_NUM; i++ )
{
if ( regVal & _BV(i) )
{
ADCValue = ( LPC_ADC->DR >> 4 ) & 0xFFF;
}
}
#if BURST_MODE
BurstCounter++;
channel_flag |= (regVal & 0xFF);
if ( (channel_flag & 0x20) == 0x20 )
{
/* All the bits in have been set, it indicates all the ADC
channels have been converted. */
LPC_ADC->CR &= ~(0x1<<16);/* Clear BURST mode, stop ADC now */
channel_flag = 0;
//ADCIntDone = 1;
adc_arr[adc_ptr] = ADCValue[5];
adc_ptr++;
if(adc_ptr >= 5000)
{
ADCIntDone = 1;
LPC_ADC->CR &= ~(0x1<<16);/* Clear BURST mode, stop ADC now */
}
else
ADCBurstRead();
}
#else
LPC_ADC->CR &= ~(0x7<<24);/* stop ADC now */
// ADCIntDone = 1;
#endif
return;
}
#endif
/*****************************************************************************
** Function name:ADCInit
**
** Descriptions:initialize ADC channel
**
** parameters:ADC clock rate
** Returned value:None
**
*****************************************************************************/
void ADCInit( uint32_t ADC_Clk )
{
uint32_t i, pclkdiv, pclk;
/* Enable CLOCK into ADC controller */
LPC_SC->PCONP |= (1 << 12);
for ( i = 0; i < ADC_NUM; i++ )
{
ADCValue = 0x0;
}
#ifADC_BURST
LPC_PINCON->PINSEL3 |= 0xF0000000;// P1.30~31, A0.4~5, function 11
LPC_PINCON->PINMODE3 &= ~0xF0000000;
LPC_PINCON->PINMODE3 |= 0xA0000000;
#endif
/*
// all the related pins are set to ADC inputs, AD0.0~7
LPC_PINCON->PINSEL0 &= ~0x000000F0;// P0.2~3, A0.6~7, function 10
LPC_PINCON->PINSEL0 |= 0x000000A0;
LPC_PINCON->PINSEL1 &= ~0x003FC000;// P0.23~26, A0.0~3, function 01
LPC_PINCON->PINSEL1 |= 0x00154000;
LPC_PINCON->PINSEL3 |= 0xF0000000;// P1.30~31, A0.4~5, function 11
// No pull-up no pull-down (function 10) on these ADC pins.
LPC_PINCON->PINMODE0 &= ~0x000000F0;
LPC_PINCON->PINMODE0 |= 0x000000A0;
LPC_PINCON->PINMODE1 &= ~0x003FC000;
LPC_PINCON->PINMODE1 |= 0x002A8000;
LPC_PINCON->PINMODE3 &= ~0xF0000000;
LPC_PINCON->PINMODE3 |= 0xA0000000;
*/
// /* all the related pins are set to ADC inputs, AD0.0~2 */
//LPC_PINCON->PINSEL1 &= ~0x000FC000;/* P0.23~25, A0.0~3, function 01 */
//LPC_PINCON->PINSEL1 |= 0x00054000;
//
///* No pull-up no pull-down (function 10) on these ADC pins. */
//LPC_PINCON->PINMODE1 &= ~0x000FC000;
//LPC_PINCON->PINMODE1 |= 0x000A8000;
/* By default, the PCLKSELx value is zero, thus, the PCLK for
all the peripherals is 1/4 of the SystemFrequency. */
/* Bit 24~25 is for ADC */
pclkdiv = (LPC_SC->PCLKSEL0 >> 24) & 0x03;
switch ( pclkdiv )
{
case 0x00:
default:
pclk = SystemCoreClock/4;
break;
case 0x01:
pclk = SystemCoreClock;
break;
case 0x02:
pclk = SystemCoreClock/2;
break;
case 0x03:
pclk = SystemCoreClock/8;
break;
}
LPC_ADC->CR = ( 0x01 << 0 ) | /* SEL=1,select channel 0~7 on ADC0 */
//( ( pclk / ADC_Clk - 1 ) << 8 ) | /* CLKDIV = Fpclk / ADC_Clk - 1 */
( 1 << 8 ) |
( 0 << 16 ) | /* BURST = 0, no BURST, software controlled */
( 0 << 17 ) | /* CLKS = 0, 11 clocks/10 bits */
( 1 << 21 ) | /* PDN = 1, normal operation */
( 0 << 24 ) | /* START = 0 A/D conversion stops */
( 0 << 27 );/* EDGE = 0 (CAP/MAT singal falling,trigger A/D conversion) */
/* If POLLING, no need to do the following */
#if ADC_INTERRUPT_FLAG
NVIC_EnableIRQ(ADC_IRQn);
#if BURST_MODE
LPC_ADC->INTEN = 0x20;/* Enable interrupts int 4 & 5 */
#else
LPC_ADC->INTEN = 0x1FF;/* Enable all interrupts */
#endif
#endif
return;
}
/*****************************************************************************
** Function name:ADCRead
**
** Descriptions:Read ADC channel
**
** parameters:Channel number
** Returned value:Value read, if interrupt driven, return channel #
**
*****************************************************************************/
uint32_t ADCRead( uint8_t channelNum )
{
#if !ADC_INTERRUPT_FLAG
uint32_t regVal, ADC_Data;
#endif
/* channel number is 0 through 7 */
if ( channelNum >= ADC_NUM )
{
channelNum = 0;/* reset channel number to 0 */
}
LPC_ADC->CR &= 0xFFFFFF00;
LPC_ADC->CR |= (1 << 24) | (1 << channelNum);
/* switch channel,start A/D convert */
#if !ADC_INTERRUPT_FLAG
while ( 1 )/* wait until end of A/D convert */
{
regVal = LPC_ADC->DR[channelNum];
/* read result of A/D conversion */
if ( regVal & ADC_DONE )
{
break;
}
}
LPC_ADC->CR &= 0xF8FFFFFF;/* stop ADC now */
// if ( regVal & ADC_OVERRUN )/* save data when it's not overrun, otherwise, return zero */
// {
//return ( 0 );
// }
ADC_Data = ( regVal >> 4 ) & 0xFFF;
return ( ADC_Data );/* return A/D conversion value */
#else
return ( channelNum );/* if it's interrupt driven, the ADC reading is
done inside the handler. so, return channel number */
#endif
}
/*****************************************************************************
** Function name:ADC0BurstRead
**
** Descriptions:Use burst mode to convert multiple channels once.
**
** parameters:None
** Returned value:None
**
*****************************************************************************/
void ADCBurstRead( void )
{
/* Start bits need to be zero before BURST mode can be set. */
if ( LPC_ADC->CR & (0x7<<24) )
{
LPC_ADC->CR &= ~(0x7<<24);
}
LPC_ADC->CR &= ~0xFF;
/* Read all channels, 0 through 7. */
LPC_ADC->CR |= 0xFF;
LPC_ADC->CR |= (0x1<<16);/* Set burst mode and start A/D convert */
return;/* the ADC reading is done inside the
handler, return 0. */
}
/*********************************************************************************
** End Of File
*********************************************************************************/
|