Content originally posted in LPCWare by nil on Fri May 22 22:35:49 MST 2015
Hi,
I am using lpcopen_2_10_keil_iar_ea_devkit_1788 free rtos code for communicating via tcip.In this project IRAM1 is selected from 0x20000000 with size 0x8000(32k).I implement the heap_4.c. in SRAM at address 0x10000000 with 50K size.My code is working well for some time (5-10min) but after that code stop executing some times i am getting error pbuf_free: p->ref > 0:650 in file ..\..\..\..\..\..\software\lwip\lwip\src\core.If anyone know about this error let me know.
thanks and regards
Nilesh