Content originally posted in LPCWare by wwwenrico on Thu Sep 17 03:58:20 MST 2015
Hi,
I'm designing a board based on the LPC1778 microcontroller.
I have to interface the LPC1778 to an external module that acts as an SSP master.
I'll configure the SSP0 interface as a slave.
The SSEL signal of the master is inverted with respect to the standard.
In fact, the idle state is 0 Volt and not 3.3 Volt.
QUESTION:
Can I use the IOCON_P1_21 register to invert the input signal and have the SSEL inverted?
Best Regards,
Enrico Migliore