Content originally posted in LPCWare by nxpsupport on Thu Apr 10 14:26:00 MST 2014
The first image looks like it has both buffers being displayed, indicating a setup/configuration problem.
Regarding the 'noise', on the 3rd image it looks like a timing issue - some lines are displayed in the wrong position, which could be caused by another bus master (especially a DMA operation, or even a LDM/STM operation) interfering with the LCD controller fetching framebuffer data. Look at the bandwidth required for the refresh settings/panel size/color depth vs the memory bandwidth (wait states, taking DRAM refresh cycles into account). What is the CPU doing? Does this happen if the CPU is executing from cache or internal RAM to stay off the bus, and no other bus masters?
Given that is it only a fraction of systems, check connections too. Noise on control & LCD clock lines/cross talk, bad solder connections, and flaky LCD connectors can also cause these issues.