Content originally posted in LPCWare by mh.hoseinzade on Thu Dec 31 06:31:24 MST 2015
Hi fiends
I'm trying to port the emWin BSP 5.22 to my LPC1788 board. However, after two weeks I was not successful.
I changed the LCDConf.c, LCDConf.h, GUIConf.h and all the needed files according to my board.
Unfortunately when I download the program to the LPC1788, It freeze and it seems that CPU can not execute GUI_Init().
In debug mode, I realized (maybe) that CPU can not exit from _I2C_Start() function. what is the problem you think?
Aso when I delete these files:
• System/HW/I2C_PCA9532.c
• System/HW/I2C_PCA9532.h
• System/HW/I2C.c
• System/HW/I2C.h
as stated in AN11218, I got some errors about the I2C functions. I don't use external eeprom and PCA9532.
Can anybody help me?