Content originally posted in LPCWare by R2D2 on Sun Feb 22 14:58:26 MST 2015
Quote: Verilog7777
I haven't written the code but that would be the true way to find out what each pin does.
And whats's not clear there?
Quote:
Chapter 17: LPC176x/5x SPI
The SPI is configured using the following registers:
1. Power: In the PCONP register (Table 46), set bit PCSPI.
...
Chapter 18: LPC176x/5x SSP0/1
The two SSP interfaces, SSP0 and SSP1 are configured using the following registers:
1. Power: In the PCONP register (Table 46), set bit PCSSP0 to enable SSP0 and bit
PCSSP1 to enable SSP1.