lpcware

In LPC1777, Is it possible to download entire code in external Flash memory and boot from that.

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Aug 7, 2018 by Priyank Bhatt
Content originally posted in LPCWare by anandana on Mon Jun 02 06:46:05 MST 2014
Hi,
         I am using LPC1777 controller, it has inbuilt memory of 512KB.  but my code size is more than 512kb. So i am planning to use external 2MB sst flash to download the code. In keil setting i have configured  for offchip start address and size. But the code is not running. Is there any other setting i need to make or In LPC1777, is it possible to download the code in external memory and boot from that. I fit is possible please guide me.

Regards
Anand

Outcomes