Content originally posted in LPCWare by leandro.stlima on Wed Jan 08 09:14:23 MST 2014
Hi fellows,
I am having a problem programming to get the data from Ethernet with LPCXPresso Board 1769. I have the same code running ok with another board using the same microprocessor but with Embedded Artist's board the code doesn't work. I can see that leds from ethernet chip work fine but there's no data coming.
I'm using the EMAC example from Micromint Lincoln e60 board and it's based on uIP code. It seems to me that this code is almost the same to the LPC board.
Has someone any idea about it? Knows this problem?
Thanks