Content originally posted in LPCWare by zavataafnan on Fri Dec 30 00:29:11 MST 2011 Is is possible to change the code for LCD 3.2 inch to support the LCD 7 inch? Is it easy or Not? couple of weeks means how many weeks?
Content originally posted in LPCWare by ktownsend on Thu Dec 15 14:56:45 MST 2011 There should be an update for the LPC1788 to also support the 4.3" and 7" displays in the next couple weeks. It will be posted on the website here as soon as it is finished and tested.