lpcware

Problem with LCD peripherals ( No LCD_ENAB_M) [ SOLVED ]

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by leform14 on Tue Jan 13 06:07:11 MST 2015
Hello,

I try to use a TFT-panel with a lpc1788. I use as reference the source code for MOD-LCD.4.3"+ evaluation board. My config are good, I see my DOTCLK at the good speed but I can't see anything on the pin 2.4 (LCD_Enable_m). The mux register is set to FUNC_7, TFT and other parameters are ok but nothing appears on my screen except ugly bar of any color. I set a buffer of y lines and x pixels that I used as UpperPanel Frame base (single mode) but nothing ...
Anybody can help me to do a check of what I have done or give me tips please ?

Outcomes