lpcware

SystemCoreClock does not compute.

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by riscy00 on Mon Jan 06 00:08:34 MST 2014
Hi

I could not get equation working correctly, I have XTAL = 8MHz and Target SystemCoreClock is 100Mhz (or close to this)

After complies and run, the SystemCoreClock provide 100.480Mhz which is okay for this application, but when I check with equation in UM10360...

#define PLL0CFG_Val           0x0004009C// This provide 100,480,000 Hz according to SystemCoreClock
#define CCLKCFG_Val           0x00000004// Divide Value for CPU Clock from PLL0 FCCO/4 = 100.48MHz as required.
N +1= 5 and
M+1 = 9D = 157
CCLKCFG=4 (post PPL divided = 4)
FIN = (Fcco*N)/2*M)
100.480MHz * 4 = 401.92Mhz = Fcco, then Fin = (401.92Mhz * 5) /  (2 * 157) = 6.4MHz…..could not compute to 8Mhz!!.

Have I missed something?








Outcomes