lpcware

LPC1788 with 800 X 480 Touch Display

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 18, 2016 by lpcware
Content originally posted in LPCWare by ridake on Sat Jun 04 05:42:20 MST 2016
              I want to use 800 x 480 Newhaven Touch Display with LPC1788. But i have one doubt about frame buffer of LPC1788, with 800x480 pixels color depth of 24 bit it requires 1.152MB of frame buffer memory, but controller has only 96KB of SRAM. So for this requirement should i use External SDRAM? or Can i able to manage with internal memory? actually i want to use LPC1788 144 pin package which does not has the External Memory Controller.

Outcomes