Content originally posted in LPCWare by MikeSimmonds on Mon Jan 14 22:18:35 MST 2013
I'm using LPCXpresso 4.3 to debug (because I am not convinced of v5 stability yet) on WinXP Prof SP3 (32 bit)
LPC1778 Custom PCB
I forgot to set the EnableDMA bit in the FIFO register when I set up my uart (Uart0)
Then I setup the RX DMA channel as if I had.
The surprising thing is that the RX DMA is working as expected -- i.e. received characters can be seen in the DMA
buffer.
Can anyone explain this or othwerwise shed light on the issue.
See also my thread "Unexpected DMA Behaviour with LPC1778".
Mike