lpcware

LCP176x pin mux tool, pin table formating

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by GRandy on Fri Aug 09 12:51:07 MST 2013
Two questions:

I see there is a pin mux tool for the LPC177x, but is there a pin mux tool for the LPC176x?

Is there a table, xls, csv, etc file available of the LPC176x different than from the datasheet?  The NXP datasheets do not format the pin tables in a way conducive to copying-and-pasting the information into a spreadsheet for easy manipulation.  When I use a spread sheet to keep track of my pin assignments, and then import that spreadsheet into my PCB design tools to define the schematic symbol, I first have to manually type (or copy and paste) the different options for each pin.  Which is a touch tedious.  Are there any better options available to me?

-Randy

Outcomes