Content originally posted in LPCWare by Elianco_ES on Mon Nov 03 13:11:19 MST 2014
Hello fellow programmers,
I'd like to configure the LPCXpresso v7.4.0 compiler
to work with Keil's MCB1700 development board which hosts NXP LPC1768 micro.
So far I used Keil's microvision5 to compile and run the programs without any problems
And it worked fine, however the free version limit is 32KB.
I also used the MBED NXP development board and it worked fine.
So I'm switching to LPCXpresso v7.4.0 compiler.
Thanks in advance for your response.