Content originally posted in LPCWare by lior.segev on Fri May 15 01:04:33 MST 2015
Hello ,
i am working on my final project to build a middleware on the LPC 176x.
i am running on the Blinky_RTX example so i can show my threads are running correctly by turning on the leds.
when i try to add the lcd and use GLCD_Initialize i get this error.
".\Flash\Blinky.axf: Error: L6218E: Undefined symbol GLCD_Initialize (referred from blinky.o)."
fro the UART i understand i don't need an include so is there an example that i can start with?
i am working with keil uvision5
Best Regards.
Lior.