Content originally posted in LPCWare by jalila211 on Fri Feb 21 07:17:31 MST 2014 hi i design a board with lpc1788 and use lcd controller for driving 15" lcd in 1024*768 resolution. by modifying CMSIS library example i can drive this lcd in 320*240 and every thing is ok. but when i change the setting to make higher resolution like 640*480 my logo image is not showed correctly. although the cursor is showed ok. in memory windows i set the one pixel color manually to red and seen that two pixel showed in screen! can any body help me?
Content originally posted in LPCWare by Pacman on Tue Mar 11 06:23:55 MST 2014 You're probably setting it to a 4-bit-per-pixel resolution. That means... writing a single byte to an address in the screen area will change two pixels at the same time.