lpcware

Implementing GPIB support on an LPC178x

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by mfogar01 on Thu Dec 13 04:08:35 MST 2012
I was wondering if anyone had any experience of implementing  support for a GPIB device on an embedded system based on an LPC178x or similar. The rough outline is that an external device acting as the master and using the GPIB interface would be plugged into a LPC178x based-board via USB. It would issue commands to the board over this interface.

So there is a need to build a GPIB "driver" on the board from the ground up or find and re-use whatever existing drivers, libraries etc. are out there. Any suggestions or pointers on this would be greatly appreciated - including commercial solutions, which may be an option if the pricing is right.

Outcomes