Content originally posted in LPCWare by reedomneck on Sun May 29 06:46:47 MST 2016
Hi,
I am using LPC1768 controller for my project and LPCxpresso IDE.
I have created 2 new projects by selecting LPCopen wizard,
For one project i have selected lpc_chip_175x_6x as LPC open chip library project from lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip file,
for second one CMSISv2p00_LPC17xx as LPC open chip library project and i am seeing difference in System control regiser.
I have mentioned it below.
In first project :sysctl_17xx_40xx.h file
typedef struct {
__IO uint32_t FLASHCFG;/*!< Offset: 0x000 (R/W) Flash Accelerator Configuration Register */
uint32_t RESERVED0[15];
In second project :LPC17xx.h file
typedef struct
{
__IO uint32_t FLASHCFG; /* Flash Accelerator Module */
uint32_t RESERVED0[31];
Can any one suggest me which one i have to select as chip lib project for LPC1768.