For the LPC435x, on page 131 of the LPC435x datasheet, the LCD panel connection table for TFT seems off. For blue bits [2:7] there are no "pin used" assignments. I'm going to hope that this is a type-o and the obvious choices for pins were just accidently not filled in. Can anyone verify?
Hi Randy,
Thanks for pointing this out! Indeed it's just a typo, nothing to worry about. I'll submit an UM/DS update request.
The obvious choices are indeed the right one, so PB_0, PB_1, PB_2, PB_3, P7_1 and P7_2 should be used for BLUE7..BLUE2
Regards,
Wouter