Content originally posted in LPCWare by mcuevas on Thu Jan 21 09:18:10 MST 2016 I just found out that EMWIN precompiled library has size restrictions on the size of my program. Whenever I use emWin_ARM7TDMI.a I get an error on my IAR system saying “Size limit exceeded (262 144 bytes).
I have the “STD” license from IAR; I should not be having size restrictions problems. I call IAR technical support to find out why I was having this error, and it turns out that emWin_ARM7TDMI.a was compiled under the “BL” AIR license which only allows 262 144 bytes.
Content originally posted in LPCWare by abigailmax on Sun May 29 01:47:40 MST 2016 I just want to display some data on LCD without using GUI_Init and other library functions (I have also observed that if I do not use GUI _Init function and just use LCD Driver files my code size is below 10K, but on using GUI_Init the code size increases to more than 55 K approx.), but by just using some basic routines from EmWin Library.