lpcware

iType font converstion

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by wendtr on Wed Jun 12 13:55:10 MST 2013

I am using emWin 5.20.  As part of emWin5.20, the iType font generator is included as an option.  In linking in the source code, it is also trying to link in the header file "fs_api.h", which does not exist.  It appears, however, that this file is included with Segger's emFile system, which is not included as part of emWin's LCD license.  This begs the question... can we use iType on LPC's implementation of emWin?  If so, where is this file?

Outcomes