lpcware

library is a ported of the emwin for lpc1768

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by engineer1 on Wed Oct 22 02:10:23 MST 2014
hi
i have a landtiger board for lpc1768.
Lcd specification:
(

Resolution:  QVGA 262K 240*RGB*320
Size: 3.2"
Controller: IL9320
Touch Panel: 4-wire
Pin Pitch: 37Pins & 1mm
2.7-3.3V operating voltage
Backlight: 5 LEDs Parallel
RSM1843 touch panel controller onboard  directly compatible with ADS7843
Standard 2.54mm PCB headers for prototyping
Support a SD card interface
)
Someone have ported library's emwin for this board?
thnks!

Outcomes