NXP free emWin library for LPC2478 ARM7 mcu is availble???.
@ECHO OFF GOTO START ****************************************************************************** * * File : Prep.bat * Parameters: None * Purpose : Sets path and other environment variables as required by tool chain * * This file is written for the IAR ARM toolchain * * It needs to be modified if the compiler is installed in a different location. * ****************************************************************************** :START ECHO PREP.BAT: Preparing environment for V850 IAR if "%_PREP_ARM_IAR_%" == "_PREP_ARM_IAR_" goto cont set _PREP_ARM_IAR_=_PREP_ARM_IAR_ SET TOOLPATH=C:\tool\C\IAR\Ew32_ARM_V3.30A\ set PATH=%TOOLPATH%\ARM\bin;%TOOLPATH%\common\bin;%PATH% SET C_INCLUDE=%TOOLPATH%\ARM\INC; :cont |
@ECHO OFF GOTO START ****************************************************************************** * * File : CC.bat * Parameters: %1 Name of file to compile (without extension; .c is added) * Purpose : Compile one file and add it to the list of files to put in * Library * * This file as is uses the IAR ARM Compiler * ****************************************************************************** :START ECHO CC.BAT: Compiling %1.c with IAR ARM compiler ICCARM -D OS_LIBMODE_DP -o temp\Output\ -s9 --library_module --cpu_mode arm --code_model small --endian little --cpu ARM7TDMI --stack_align 8 --interwork -e --require_prototypes --silent temp\Source\%1.c IF ERRORLEVEL 1 PAUSE ECHO temp\Output\%1.r79>>temp\Lib.DAT |
@ECHO OFF GOTO START ****************************************************************************** * * File : Lib.bat * Parameters: None * Purpose : Put all (object) files in linklist into the library * * This file is written for IAR ARM tool chain * ****************************************************************************** :START ECHO MAKELIB.BAT: Creating GUI target library using IAR ARM tool-chain REM **************************************** REM Create library REM **************************************** IF EXIST Lib\GUI_TARGET.LIB DEL Lib\GUI_TARGET.LIB xar lib\GUI.r79 -x temp\lib.dat IF ERRORLEVEL 1 PAUSE |
Yes. Use ARM7TDMI core library.