Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 31 12:09:58 MST 2015
Quote: denn4208
So I just installed on a windows machine and it is there in the windows version, but not in the linux version.
Then I'd recommend you reinstall on Linux. I just checked a clean LPCXpresso_7.9.0_455 installation on Linux. If I create a LPC15xx project through the project wizard, I don't see a problem. For existing LPC15xx projects, I can open Properties -> C/C++ Build -> MCU settings and see all supported LPC15xx variants.
Thanks and regards,
LPCXpresso Support