Content originally posted in LPCWare by mc on Thu Aug 14 17:21:00 MST 2014
Hi ramniraj1,
In LQFP100 package, all 28 PWMs are available at the pins. Although SCT0 and SCT1 has 10 outputs each, all of them are not coming out to pins.
See below break-up.
SCT0 -> (Out0 to Out7) -> 8 Outputs connected to pins
SCT1 -> (Out0 to Out7) -> 8 Outputs connected to pins
SCT2 -> (Out0 to Out5) -> 6 Outputs connected to pins
SCT3 -> (Out0 to Out5) -> 6 Outputs connected to pins
--------------------------------------------------------------------------------------
Total SCT outputs -> 8+8+6+6 =28 connected to pins