Content originally posted in LPCWare by afiqahlaa on Mon Aug 03 20:46:35 MST 2015 Good morning and hye!
I am wondering, do I need any Debugger Probe for be to debug code using IAR IDE for board LPC1549? FYI, I am using LPC1549 together with rev. B board which is demo board of OM13067. http://www.nxp.com/demoboard/OM13067.html
Content originally posted in LPCWare by lpcxpresso-support on Tue Aug 04 00:32:02 MST 2015 Soft booting of the debug probe is only supported using LPCXpresso IDE. For use with IAR, you'll need to program CMSIS-DAP or J-Link firmware into the on board debug probe's flash, which can be done using LPCScrypt. For information on this see: