Using ISP "G 0 T" command on LPC1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using ISP "G 0 T" command on LPC1549

428 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by randyd on Thu Nov 27 14:32:30 MST 2014
Hello,

I've written a factory programer in Python to serial ISP flash our LPC1549 and LPC1115.
After flashing, the LPC1115 user code can be started without a power cycle or reset symply by issuing the "G 0 T" ISP command,
however this does not work with the LPC1549 and it appears to hang, I've also tried "G 0 A".
I'm unable to find what the difference is after reading the user manuals, if someone could point me to another appnote or give advice I'd appreciate it.
Thanks,
Randall.
Labels (1)
0 Kudos
0 Replies