Hi,
The Beekit does not utilize the Codewarrior projec wizard, so you can not follow that approach.
If you must use the Float format, then you must replace the ansiis.lib with e.g. The anisfs.lib which will include the functions needed for using the "float" and double variable type.
The codewarrior help clearly specifies what features the different libs support (seach for ansi library reference)
It is common knowledge that using floating point in small CPU's is a very bad idea as it takes up too much code space.
Therefor it is easier to use real numbers and then scale you input if possible.
Br,
Mads